You are here: Understanding KAS > Motion Concepts > Pipe Network Concept > Pipe Network

Pipe Network

To control the machine application with multi axes that are dynamically interconnected, you can design several pipes with the KAS IDE"Integrated development environment" An integrated development environment is a type of computer software that assists computer programmers in developing software. IDEs normally consist of a source code editor, a compiler and/or interpreter, build-automation tools, and a debugger to create the global Pipe Network as shown in Pipe Network Structure.

Relationships between the Axes are developed and connected graphically, allowing you to visualize how the machine functions. Each horizontal flow is considered as a separate pipe. In the application below there are three pipes.

Concept Link IconSee Also

 


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™